Por favor seleccione el país de entrega adecuado

Algunos factores como el precio de los productos, su disponibilidad u otros servicios pueden verse afectados por la selección del país de entrega.

Chemist prescription printer

Precise and effective

This prescription printer, which is used in pharmacies, fits into the limited space of a cash desk drawer. The printer is one of the most important components of the cash desk, as failure prevents prescriptions from being processed and thus means a sales shortfall. Absolute accuracy is also required for a precise typeface. The ink cartridge holder slides on the metal guide rod with two iglidur® J plain bearings, whilst two additional guides on the metal lip help it to run parallel. The guide rod was assembled with igus® MCM clip bearings.

Thorbjörn Missalek, JDM Innovation GmbH, Murr

More on applied products here

Further interesting applications from extremely diverse areas can be found here.



Consultas

Estaré encantado de responder a sus preguntas personalmente

Consultas y envíos

En persona:

De lunes a viernes de 8:00 a 18:00h

Online:

24h