Today, the round drylin WS-16 single rail is used in the seat adjustment mechanism. The seat can be adjusted easily to the respective body size without tools. The maintenance-free rail solution with two quick-release mechanisms replaces screws that had too much play during riding.
Quick linkage folding uses igubal plastic rod ends with such features as high fatigue strength under changing loads.
The rod ends also compensate for edge loads and misalignments. This prevents the entire system from wobbling when it is being folded out.
The transportable drylin W-measuring system has been used for over a year for base frame spatial measurement. There are plans to transfer the variable system to the suppliers as well.
The economical all-round plain bearing made of iglidur G plain bearing, which is suitable for almost any application, also exhibits its multifunctionality in the bicycles. Insensitive to dirt, it proves its strength under high loads in the pedals and in the seat suspension. The PMA protective hose guides the motor cable and the front and rear hydraulic brake lines in a reliable manner.
Finally, the arm is correctly positioned and can still follow the movements of the body: smoothly gliding forwards and backwards, outwards and in front of the body. The light, flexible drylin N40 low profile guide system is used in the sliding rail.
The plastic bearings' long service life, low weight, corrosion resistance and the lack of lubrication required also played an important role for the special bike manufacturer, making these decisive factors in purchasing.